Hello
I am using LP5907SNX-2.7/NOPB regulator in my design. the Input to the regulator is 3.3V, output is 2.7V and enable pin connected to 1.1V. Enable pin minimum threshold high voltage mentioned in datasheet is 1.2V nad also in the datasheet Figure 2. VEN Thresholds vs VIN showing that with 0.8V also the regulator will turn on. I need to connect ENABLE pin to 1.1V because of the power sequence requirement.
Can you please confirm 1.1V to the enable pin will work or not?
Thanks
Mani