This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40210: 12VDC to 100VDC converter

Part Number: TPS40210


Hi,

I used WEBENCH Design tool to design a DC/DC converter 

My question is "Can I use cermaic capacitor array 5x 10uF 50V instead of 33uF 250V Aluminium Electrolytic Capacitor because I have a problem with size of 33uF capacitor" ?

  • The AL Elect cap also serves as boot of storage and damping of the output filter. Ceramic and L will produce a high Q filter which must be damped for stability concerns. If you can close your loop to a lower bandwidth, you may be okay with only the ceramic caps. Otherwise, you will need to do something damping. Check if a 10uF AL ELEC cap can fit.