Other Parts Discussed in Thread: TPS3711, TPS3701, TL7700
Hi team,
Do we have solution to replace MAX16053AUT?
Customer VCC is 19V input.
Thanks,
SHH
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
SHH,
We have a couple devices that operate at 19V (up to 36V) which is:
1. TPS3711 which is a voltage detector (no delay)
2. TPS3701 which is a voltage detector with both undervoltage and overvoltage monitoring.
We do not have a device that operates up to 19V with enable and programmable delay unfortunately at this time.
Please click “This resolved my issue” button if the answer provided resolved your issue.
-Michael