Hi team,
Is there any concern about switching the current limit with the H/L pin while the part is loaded? We're running into some issues when we transition from 100mA to the 500mA limit, which happens while the part is switching. When this happens the part stops switching, but stays on so the output voltage rises up to 4V (output should be 3.3V nominal)
Here are a view scope shots to show the behavior
Ignore the labels on the scope shots, the channels are labeled as follows:
Image CURRENT 1.PNG:
Trace 1 is the output voltage.
Trace 2 is the H/L control pin 3.
Trace 3 is the USB 5V input current to the regulator.
You can see that approximately 620msec after turn power was applied trace two transitions low to high (0>>5V) which should transition from the low to high current limit. At this point you can also see that the voltage on the output steps up, very puzzling.
Image CURRENT 2.PNG:
This image shows the same trace 1 and 3 as in CURRENT 1.PNG above but trace 2 is now the switching side of the inductor. You can see that at the 620msec transition period of the low to high on pin 3 the regulator stops switching.
Image LOW TO HIGH TRANSTITION 3.PNG:
This image shows the same traces as in CURRENT 2.PNG but at a higher resolution. We did this to show that we do not think the device is current limiting during this transition period. You can see where the switching waveform stops which is when we control the low to high transition on pin 3.
Thanks!
Nate