This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV733P: Over Temp cycling time?

Part Number: TLV733P

I have a customer running a series of test on a TLV73318PDQNR in their system.  At an elevated 80C ambient temp and a deliberate fault condition of 350mA overload instead of expected current foldback the output goes to zero and appears to shutdown.  However, once the overload is removed the device starts up "almost instantly".  The input voltage is 3.3V so obviously they are hitting thermal shutdown but the question is why does the device restart so quickly once the overload is removed?  The nominal load is between 150mA and 280mA.  What timing would you expect for thermal restart given the thermal hysteresis is 20C?

Thanks!

  • Hi Allen,

    The thermal restart time is going to vary based on the ambient temperature, but it is typically a couple of milliseconds. Is the 350mA load electronic or resistive? If you are using an electronic load it may be getting stuck in foldback current limit, if this happens as soon as the fault is removed the part will startup almost instantly. You should be able to tell if it is stuck in foldback if you look at the supply current.

    Best Regards,
    Mark