I have a design using an OMAP3530 and TPS65950 development board. The system is turned on and off by supplying VBAT to the TPS from an external regulator (the backup battery is not connected). I have a problem where even though I am not supplying VBAT from my system, the VBAT power rail is partially powered up to 1.2V when VBUS power is present on the OTG port. It seems like the TPS chip is trying to charge up the VBAT power rail from VBUS. Currently, the BCI is configured to support charging. If I change the circuit to match Figure 8-3 (Typical Application Schematic BCI Not Used) in the TPS65950 Data Manual, will it stop powering up VBAT from VBUS?
Thanks,
Ryan