This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV61046A: DC/DC boost converter

Part Number: TLV61046A

The DC/DC Boost converter has an Enable pin to switch the device in shutdown mode. My confusion here is, what will be the logic levels for this? My input to the Boost converter will be 2.5 volt, and the output is 12 V. So the high logic level will be 2.5 Volts or 12 Volts?