This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ20Z95: Fully Charged Bit

Part Number: BQ20Z95

Hi All

Does anybody know how the fully charged (FC) bit is set in the battey status register for the bq20z95 batttery management controller when the FCA SET% is disabled (-1)?

Regards

Stephen

  • if FC set% is programmed to any other value other than -1%, the flag will get set once the SOC reaches that value. If set to -1, then FC will get set based on primary charge termination conditions i.e taper current and taper voltage conditions. See TRM.
    thanks
    Onyx