This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'm struggling to get I2C communication working on the BQ25703AEVM-732 board. On close inspection of the board, it would seem that the wrong IC is populated on the board.
On the part it reads (as best as I can read it) :
PQ25700
AA0
TI 738
A06C
Surely this should be 25703? On the eval board itself it clearly states that this is the 25703 board? Could there have been some mistake here or am I missing something?
Thanks
Kilian
Hi, thanks for the help.
I don't have the EV2400 module so I'm using a micro-controller to communicate with the eval board. I'm trying to read the Manufacturer ID from 0x2E register, it should return 0x0040 but I seem to get 0x4078 instead which is what the micro reads and I also read it manually from the oscilloscope.
Here's what I'm seeing on the scope.
Any idea what I'm doing wrong here?
Thanks
Kilian