This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61046: Enable Pin Question

Part Number: TPS61046

Hi,

I designed a circuit with TPS61046 and I didn't understand correctly the Enable pin voltage levels 
(page 5 in the data sheet) 
It is written that the maximum  Ven_H votage treshold is 1V, And the minimum Ven_L voltage treshold is 0.4V 
I think it is a mistake the 1V should be the minimum for Ven_H and 0.4V should be the maximum of Ven_L (Am I right???)


My question is, Can I connect the enable pin to Vin (I think I can,but I have some doubts...)? 
Vin in my circuit is 5V.

Please help

Thanks,

Moshe Eitan