This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: The Different between Qmax update and Fast Qmax update? What is the accuracy different between Qmax and Fast Qmax?

Part Number: BQ40Z50-R1

1.Normal Qmax calculated as Qmax= PassedCharge / (DOD2– DOD1), how Fast Qmax calculated?

2.What is the accuracy for Qmax update and Fast Qmax update?

  • 1.It is still pretty much the same formular, just that in this case, qmax uses DOD@EOC as one of the DOD points( if there isn't a DOD0 point taken) and then the other will be a DOD calculated after you are at a certain SOC closer to the end of discharge, typically after 15% SOC...
    2. The error in qmax with fast qmax update is usually less than 2%. With regular qmax update, it is less than 1%

    thanks
    Onyx