helleo , I need to drive a laser diode array, total 8 strings , each string voltage about 35V, constant current 2.5A(typical), 3A(max), TPS92660 can be current trimmed by I2C interface, and achieve PWM current, it is good for me. Now I have some questions for TPS92660:
-
Its Iout ( max )is 5A from TI website . This is buck converter out current, right? The linear regulator max out current?
-
About the buck converter out current trim, if I set out current is 2.5A, the current change -20% should be 2A, 32 steps from 2.5A to 2A, each step change about 0.6%(about 0.015A); the current change 19.4% should be 2.985A, 32 steps from 2.5A to 2.985A, each step change about 0.6%(about 0.015A); right?
-
If I parallel 8 stings LD at an output voltage, is that okay? Will there be interference between them?
Do you have any suggestions or good solutions for my application?