This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40428: TPS40428 with CSD95378BQ5MT - Current limit for 2 phase operation

Part Number: TPS40428


Hello,

What is the current limit of the TPS40428 when working with the Smart FET CSD95378BQ5MT?

According to the Webench its 60A.

The data sheet and the Fusion SW current limit is 50A.

On the other hand the data sheet clearly indicate that with 4 phases it is possible to get up to 120A, so for 2 phase it should be 60A.

I need to set the fault current limit to 60A and the warning limit to 55A. Is it possible?

Is it possible to add voltage divider on the IOUT signals of the CSD95378BQ5MTtowards the TPS40428 in order for the TPS40428 to actually limit a higher current?

Thanks and Best Regards,

Yossi