This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25606: Do I need USB data for the charger controller

Part Number: BQ25606

Do I need the USB data lines to use the BQ25606, or can i just apply 5V to the power input? Maybe I can use a short or some resistor divider across the datalines? I only need 0.5A max for my application? Thanks.