Hello,
I am somewhat confused by the default behavior of this part. By default,am I correct in saying the FET action is disabled? I am using the eval board and after much work I managed to get the two FETS enabled. What confuses me is that if these two FETs are disabled by default, the battery in the circuit would be disconnected from its load, which in a typical situation could be a host MCU. If in this case the host MCU can never power on to program the registers on the bq28z610, how is the system supposed to start without pre-programming the bq28z610 when populating the board? Am I missing something here?
Thanks,
Kilian