Other Parts Discussed in Thread: TPS23756EVM, TIDA-00465, TPS23756
Hi Everyone!
I've used only the single port of "TPS23861" in Auto mode configured with iMX6 as host processor. I used "TPS23756EVM" as PD to test the functionality of our design. I am facing issue that whatever is the classification resistor i'm using at "R9" in TPS23756EVM, it's always showing the class 0 at CLI and there is always one event classification happening irrespective of the CLS resistor value i used at "R9" on PD. If i'm not wrong there should be 2-event classification when the PD used is class 4 (802.3at compliant).
If i connect a load more than 15W the PSE limits the port current to ILIM current limit which is changing from class 0 to class 3 with the corresponding R9 value at PD. But, It's not sourcing the 802.3at mode current to a valid class 4 PD. I want to use our PSE controller in auto mode as the PD could either be 802.3af or 802.3at compliant.
Please tell me why it's not detecting a class 4 PD accurately. Please let me know if there is anything i'm missing in hardware or software configuration.