Hi.
I'm looking for a power mux that can handle two inputs automatic switching:
1. 4.5 - 17V, 4A max (adapter).
2. 3 - 4.2V, 4A max (Battery).
The output should follow on the higher voltage input.
The output Current should be 4A max.
Can you please provide a suitable integrated solution?
BR,
Gilad.