This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SWITCHERPRO: Calculated maximum value in analysis window

Part Number: SWITCHERPRO

Hi,

In switcherPro, I am checking the characteristics of TPS53355 for 12V input and 0.95V output.

In analysis window( as shown in attached image), there is a column: Calculated Maximum.

That value is 1.905V, which is very much grater than 0.95V.

So i would like to know what does this indicate.

Regards,

Madhu