Tool/software: WEBENCH® Design Tools
Hi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: WEBENCH® Design Tools
Hi
I tried this. I entered Vin = 15 V, Vout = 10.5 V and Iout = 8 A into the default screen on theTPS54824 product page. Webench creates the design. I went to the advanced options on the left hand side and manually entered 500 kHz switching frequency. Webench re-created the design with no issues.
I apologize for my lack of explanation.
I simulated TPS54824 at Ta=90℃.
Best regards,
Yokota
Webench limits the junction temperature to 125 C. Higher switching frequency means more switching losses so Webench limits the frequency range based on junction temperature.
Hi