This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54240: coupled inductor

Part Number: TPS54240


Hello

I got this PSU design around the TPS54240, basically it is the same design shown on the app.note SLVA369A (http://www.ti.com/lit/an/slva369a/slva369a.pdf), that uses this DC converter to get positive and negative outputs.

I need to select a different coupled inductor. At this time it is using a custom (not commercially available) coupled inductor with these specs:

I'd like to use a commercial inductor (available on Mouser or similar). Can anyone help me identify a similar part that would match the performances, or at least come close?

I'm a computer engineer, not an electrical engineer, so the best I could do is select those possible inductors, but I'm totally not sure about how they would perform. I simply choose a coupled 22uH inductor since the original one is 21uH/25uH.

1) https://www.vishay.com/docs/34359/ihcl-4040dz-5a22.pdf

2) http://www.mouser.it/Search/m_ProductDetail.aspx?Coilcraft%2fMSD1260-223MLB%2f&qs=zCSbvcPd3pa32vh7IhFCEQ==

Also I have the following questions:

- would this PSU design work if only the negative output is actually used, and not the positive?

- what is the positive and negative voltages before the two LDO regulators?