Hi Team,
I got an inquiry from one of my customers where they need a boost controller with an input of 12V to an output of 24V, 2A. They also need the feature of true shut down during a fault to protect the load from the main line. I have proposed our LM3017. I just wanted to confirm if this part can support an output of 24V and 2A. I tried in webench but faced errors but was able to make a design with 1.5A instead. Can you confirm if the LM3017 is capable of this?
Thanks!
Best regards,
Alfred