We need something which can limit o/p current of the negative regulator LM27761 (-3.5V) to 10mA after 10mA current should not increase.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We need something which can limit o/p current of the negative regulator LM27761 (-3.5V) to 10mA after 10mA current should not increase.
Hi Rahul,
Just to clarify, are you looking for a switch that can be placed in the power path of the LM27761 that will limit the current of the device to 10mA? If this is a -3.5V application, then we do not have any integrated load swiches or eFuses that can handle negative voltage.
Thanks,
Alek Kaknevicius