This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61200: Max Duty

Part Number: TPS61200

Hi,

We got a question from customer about TPS61200.
Could you help us?

[Question]
How much is the variation of max Duty at all over the temperature? They are considering using under the following condition.

 Vin min=1.1V
 Vout=5.5V
 Iout=100mA

Best Regards,
tateo