This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2115A: switching between input sources

Part Number: TPS2115A
Other Parts Discussed in Thread: TPS2113A

Hi

 I am using TPS2115A to switch between battery-1 and battery-2. Can I use the same product to implement the switch between input from wall and battery-1?

  • Hi Padmapriya,

    The TPS2115A does not distinguish between power supply types, so using the device for a wall adaptor instead of a battery should work. If you would like to further customize your solution, you could use the sense pin of the TPS2113A to set the threshold for automatic switching.

    Thanks,

    Alek Kaknevicius