Other Parts Discussed in Thread: TPS782, TPS706, TPS727
Trying to find a close second source to Analog Devices , ADP160ACBZ-1.8-R7. Key is Iq at low load current of 1uA where it spends most of the time, then when device wakes up for 20 seconds the load current is 100mA then back to sleep. Therefore the regulator quiescent current should be on the order of the load current for long battery life.