This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/BQ40Z50-R1: calibration bq40z50-r1

Part Number: BQ40Z50-R1
Other Parts Discussed in Thread: BQSTUDIO, BQ40Z50

Tool/software: WEBENCH® Design Tools

Hello everyone;

I started configuring the bq40z50-r1 with bqstudio. I followed the apllication SLUA734A (bq40zxx Manufacture, Production, and Calibration). The worry is that it explains that it is necessary to send a command but in bqstudio the commands are predefined. The one requested to be carried out is not part of this list.
Do you have a solution ?

bq40z50_r1_test1.gg.gg (2).zipAnother question the chemistry file contains all information about the battery not?
They are automatically updated in the regsitres?

best regard 

Anthony 

  • Pls use the advance comm SMB tab of bqstudio to send any command that isn't predefined in the command window.

    As long as you have identified your chem id, program it on the gauge using the chemistry tab, then perform a learning cycle. This will allow the gauge to accurately track SOC. You need to extract an srec from the device which will be your golden file used to program multiple gauges.

    thanks
    Onyx