This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5175: Unstable issue at higher load current

Part Number: LM5175


Hi,

I have a prototype of a LM5175 board which seems to get unstable at higher load currents, also the load response is not very good.

Input voltage is from 5,5V to 20V with an output voltage from 8,1V with 4A load current.

I use 4 BSZ065 from infineon and a 3,3µH coil at 600kHz. Is it possible to provide a schematic and other relevant data outside of this public forum?