This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54320: TPS54320 the EN pin input signal

Part Number: TPS54320


Hi ,

I have a question about TPS54320.

Now, I want to controll the EN pin by the external signal.

Datasheet say if an application requires controlling the EN pin, use an open-drain output logic to interface with the EN pin.

Can we input High/Low signal directly to the EN pin?
Is the EN pin required a external pull down resistor ?

  • It is ok to drive the EN pin directly with a high/low signal. You may need a pull down resistor but it depends on the characteristics of what you plan to drive the pin with and the desired behavior.

    The EN pin has an internal current source of ~1 µA which will pull up the pin if it is left floating. This is why the datasheet mentions driving it with an open-drain logic signal. Open-drain logic would be able to pull EN low to disable the part. When the open-drain logic goes high-impedance, the internal current source pulls up the EN pin to enable the TPS54320.

    If you want to make sure the part is only enabled by your high/low signal and you cannot guarantee what is generating the signal to drive EN will always have drive capability to pull EN down, I suggest adding a 100 kΩ pull-down resistor.