Hi...
My customer is verifying the performance of TLV62585 and asked some questions as follows.
1. Why does this voltage step like red arrow of Picture 1. cause?
2. I think that fluctuation of input voltage can be caused by inrush current from output load capacitance. Is it right?
3. What is recommended output load capacitance range? (expected output load capacitance is 30uF to 90uF)
4. If inrush current is occurred at voltage step period, can input or output voltage power rail be damaged or not?
Picture 1. Start-up waveform without load of TLV62585
Please let me know that.
Thanks.