In page 14 of DS, it mentioned the balance current for external circuit. I am confused if the equation is simplifed or not.
Need you comments to provide more detail for Icb1 and Icb2 in exnteral circuit.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In page 14 of DS, it mentioned the balance current for external circuit. I am confused if the equation is simplifed or not.
Need you comments to provide more detail for Icb1 and Icb2 in exnteral circuit.
Hi Vish,
What I need to put more comments is Fig.11 in DS. I am confused the equation of balance current.
Vish, your calculation for the balancing current makes much more sense than the one in the datasheet:
For me it makes absolutely no sense why RCB1 and RBC2 should influence the balancing current. As far as I see they are only for the RC low-pass filter for the comparators.
Can you confirm, taht the formula in the datasheet is wrong? And what do you expect for RGS_ON (Rint in your image)? 150mOhm?
Edit: The error has been introduced between Revision A (September 2010) and Revision B (December 2014)
Edit2: And for the record: between RevB and RevC the Mosfet Type for external cell balancer changed from enhancement type to depletion type (I guess Rev.C is wrong here, right?)
Thank you, Andy