Other Parts Discussed in Thread: TPS55010, TPS62135
Hi, team.
My customer is looking for an alternative to BD7F100EFJ-LBE2 (made by ROHM).
This application's specification is "12V(2W@MAX)⇒ISO DCDC⇒12 V".
But, my customer is considering diversion to another application, too.
(Its specification is "12V⇒ISO DCDC⇒5V")
I have been introducing TPS62110RSAR with reference to the document of PMP20450, but please let me teach because got a question from the customer.
※If you can answer "usable" it seems that the considering will be progressing.
<Customer Question>
TPS62110 is a normal synchronous rectifier converter.
① I think that this IC is not an insulation dedicated IC, but can it be used?
If the answer is "YES" please tell me following under.
② Difference in internal structure with DC-DC dedicated for insulation by competitor product
③ The risks (demerit) when used for isolation.
④ Installation result used for isolation.
Could you help me?
Best regards,
Masumi Sekiguchi