Is there a link between the RST_TH reference (0.8V) and the feedback reference (2.5V). Are they ratiometric with each other. If so there should be a % tolerance shift between the two that should be better than the absolute tolerance of each one that is given in the data sheet. The absolute tolerance of 0.8V given in the data sheet is 4%. The tolerance of 2.5V is 1.5%. Am I allowed to assume that the tolerance between 0.8V and 2.5V is no worse than 4%. Thanks.