Other Parts Discussed in Thread: LM5170
I have been tasked with creating a converter which can transfer all the energy from one storage device to another.
The full storage device has a voltage range of 18V when full to 6V when empty
the target device has a terminal voltage of 0V when empty and 18V when full (so needs CCCV control)
I need a transfer current of 50A or more.
The demo board looks very interesting but I'm unsure if it can do what I need.
I don't need isolation or bidirectional.
Thanks