I am interested in this IC (tps7a85a). In section 8.1.1.1 it is mentioned that "R1 and R2 can be calculated for any output voltage range using . This resistive network must provide a current equal to or greater than 5 μA for dc accuracy. TI recommends using an R1 approximately 12 kΩ to optimize the noise and PSRR."
Is it mandatory to have R1 to be around 12.1Kohms? Can I use some other value (say 1K-6K) as long as I maintain resistive current equal to or greater than 5uA?
Example: to achieve 0.9V in adjustable mode, I would like to use R1=5K and R2=40K. Is this fine?