This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tps65130: i need single input dual output output

Part Number: TPS65130
Other Parts Discussed in Thread: TPS65131, TPS54140, TPS54160A

i need   single input dual output  

 input voltage  is 5V (Vbus)

output volatge range  is  -15V to +15V

Current is not mandatory  consider above 500 mA

i selected from TI    TPS65130  but i need alternate part why because this part cost is high and internal circuit to large that 's why is not suitable to our applications please suggest me alternate part number and low cost and small circuit.