Other Parts Discussed in Thread: LM5165
My application
Motor as a generator ---- bridge rectifier --- single op-amp V and I monitor to control maximum power transfer ---- Buck converter ---- supper-capacitor----- Boost converter ---- 3.3V out
I am considering using TPS62125 because of its efficiency and low voltage operation but I am concerned about what the current drawn from the super-capacitor when there is no input power.
If it were 30uA say? that would be fine but if the regulator goes into some output discharge mode that would be a problem. I want to avoid adding diodes as these would limit the minimum operating voltage.