Hello, I'm planning to use BQ25606RGE as a battery charger and power supplier for my system.
My 12V 1A wall adapter is the primary source and will be connected to VBUS of BQ25606.
After that , it will charge LI-PO battery and provide Vsys rail for my devices through BQ25606.
By the way, I don't need any USB related things such as OTG, D+, D- pins.
Datasheet says 1. I can limit input current through ILIM pin if I don't use D+, D- pins 2. OTG pin should not be floated.
Here are my questions.
1. In this case what should I do to those pins(OTG, D+, D-)? (My expectation is to make OTG grounded and D+ D- shorted)
2. Does Boost mode mean Vsys is boosted up to 5.15V and support current up to 1.2A??