Part Number: LMR16020
Hi friends,
I have my doubt about the formula of output capacitor in the datasheet as attached.
If IOH=2A, IOL=0.2A, Vout=50v, Vos=250mV, L=9.55uH, the value that I calculated based on equation 12 is 108uF(fsw=200k),not 36uF, and the value that I calculated based on equation 13 is 1.5089uF, not 7.7uF, did I misunderstand? Please kindly explain the formula for me.
Best Regards,
Thanks