Hi,
pls find below customer issue using bq20z45-r1 in production:
BQ20z45-R1 fuel gauge implemented in 2s4p batteries (just after production) send RSoC value with +5% to +8% error after they are partially charged (from 30% to 50%).
Partial charging occurs just after production, batteries have never been fully charged but they are storaged several weeks.
RSoC error have been estimated comparing RSoC on SBS data sent by the fuel gauge and voltage characteristic (Voc = f(SoC)) of the cell used.
RM and FCC updates after Impedance Track launch (exit of relaxation mode or 5h after a short discharge) give no improvement.
A full charge or full discharge removes RSoC error.
Is this RSoC error is due to the partial charge of batteries that have never been fully charged ?
Parameters in dataflash called Cell 0..3 Chg DOD at EOC are at 0 on batteries that have never been fully charged, can we simulate a fully charge by increasing this value >0 ?
thanks in advance for your support.
Paul