This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24074: Need help selecting a battery charger IC

Part Number: BQ24074
Other Parts Discussed in Thread: BQ25120, BQ24230

Hello,

   I have a medium sized wearable device that I need help selecting a battery charger IC for.

System current: 80mA (processor, radio, etc.). The output of the charging system will feed an LDO to drop the voltage down to 3.3V; unless there's a charger that has a built-in 100mA LDO.

Battery Type: Li-Poly, 400mAh, 3.7V nominal voltage. Charge Voltage 4.2V.

For ease of prototyping we're going to start with this battery.

What charger IC? Charge speed doesn't matter, as long as it's done within 8 hours.

The BQ24074 looked interesting, but I don't know if the voltages and currents work out, and if it's overkill for this simple application.

Thanks in advance,

Derek