Hello,
I'm building a Qi receiver based on the BQ51003 and the WR301025-19M8-G coil from TDK. I've calculated the C1 and C2 according to the instructions specified on the BQ51003 datasheet, which resulted in the following theoretical capacitors:
C1 = 0.833962uF and C2 = 0.009426uF
Practically, I'm using the following capacitor values C1 = 0.47u+0.22u+0.1u+0.047u = 0.837uF and C2 = 8200p+1200p+18p=9418pF.
When I test my receiver with the AVID Qi FOD Transmitter v1.1 I repeatedly get the Device Detected message in the serial port (signal strenght between 55 and 59), and only if I very finely position the receiver on the transmitter the system passes from the Device Detected message into the FOD power transmission messages.
I'm assuming that this behaviour is related with a problem in the communication between the receiver and transmitter, which could be optimized by fine tuning C1 and C2. My question is: how can I do that fine tuning?
Thanks,
Carlos