Hello Team,
My customer starts to design TPS40140 schematic and they don't know how to design the compensator circuit. Could team can provide a initial setting that customer can start with it and fine tune the setting by checking the bode plot.
Customer's circuit setting as below, please let me know if any other information is needed.
Two phase single output
Vin=7V~14V
Vout=0.7V~1.8V
Iout=60A
Frequency=500kHz
L=0.2uH
Cin=22uF*8 (GRM31CR61E226K)
Cout=470uF*4 (2R5TPE470M9)+47uF*8 (GRM31CR60J476M)
Thanks a lot.
Vincent Chen