Other Parts Discussed in Thread: LM5175
Hello All,
I came across TPS40170, which I wish to use in my application as DC\DC buck converter. I plan to use it in Automotive application. The aim is also to monitor the input currents. As it will be connected to Vbatt (12V-48V)
Does this Switching regulator (regulation IC ) deal with digital input interface ,if it is SPI interface?
Is it possible to use for the feedback not from the output, instead from the input ? , used by IC to control its output
Regards
Bhargav