This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100-G1: Is VEN pin pulse duration configurable ?

Part Number: BQ34Z100-G1

Hi,

I am using the BQ34Z100-G1 on a custom electronic board.

When my board is only powered by the battery, I use the VEN pin to activate voltage divider only during the measurement by the gauge (the gauge is in SLEEP mode or FULL SLEEP Mode), this is working fine.

However, when my board is powered by an external source (battery is charging, gauge is in NORMAL Mode), I would like to force VEN pin to be continuously high. (Because I am using the voltage divider for an other part of my schematic)
Is it possible? How can I do that ?

Currently, in NORMAL Mode, I see a 125ms pulse every 1000ms, my aim is to get this pulse larger or if possible continously at high level.

Thanks for your help.

Flavien