Tool/software: WEBENCH® Design Tools
Hi Team,
We carried out simulation at the following conditions.
However, we were not able to obtain an appropriate result.
<conditions>
VIN=12V
VOUT=1.0V
IOUT=0.2A ⇔ 2A
Fsw=2.5MHz setting
Soft Start time = 0.2ms
By the way, we were able to obtain an appropriate result at the following conditions.
<conditions>
VIN=12V
VOUT=3.3V
IOUT=0.2A ⇔ 2A
Fsw=2.5MHz setting
Soft Start time = 0.2ms
Is this phenomenon the bug of WEBENCH?
If yes, Can you improve this problem?
Regards,
Kanemaru