This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53647EVM-710: The device can't be found by FUSION_DIGITAL_POWER_DESIGNER

Part Number: TPS53647EVM-710


Hello, sir

I want to use TPS53647EVM-710 to do some tests. But when I lanched  FUSION_DIGITAL_POWER_DESIGNER(v7.0.18), the soft can't find the device.

I'm sure that the power supply of the board is correct. And the EVM has been tested before, which means the board is OK.

I really need a help. Thank you!

Best regards!

Wei Guo

  • Hi Wei,

    When you launch FUISION_DIGITAL_POWER_DESIGNER, if you can not find the device, please go to "Change Device Scanning Options" and select "Device Code",  hit "OK" and come back to previous screen, and then "Retry" you should be able to see the device.

    Regards,

    Weidong