This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: Writing directly to registers

Part Number: BQ40Z50-R1
Other Parts Discussed in Thread: BQ40Z50

I need to programmatically change values in the LED Configuration (0x47F2) during Final Testing.

I need to change the value from "00 17" to "00 13", run some tests and then change it back to "00 17"

Is there a way to do this?

Thanks,

Larry