This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53667: About the Function of TPS53667

Part Number: TPS53667
Other Parts Discussed in Thread: TPS53681

Dears,

       Can you help to double check the function about tps53668,

       Customer need a 6-phase Analog PWM controller to design a 12v to 0.84v/140A power ,tps53667 is suitable for the below demand? Thank you very much.

1.12 V to 0.84V,(0.8 V to 0.8 V adj.), Iout=140A, the output cannot be experienced overshoot process.
2.6 phase PWM analog PID controller.
3.With PMBus ,can remote transmission.
4.Ripple 1%@20Mhz.
5.Voltage regulation accuracy:±0.25%.
6.Dynamic:±3%(140A step)
7.Environment temperature:-10℃~55℃.
8.Environment speed: 200LFMtps53667.pdf