This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC29002: UCC29002 & UCC29002-1

Part Number: UCC29002


Hi All,

What is the difference between the two device ?? UCC29002 and UCC29002-1.

  • Hello Pao Wu,

    The UCC29002 has startup logic where the LS driver is disable and the ADJ amplifier is forced to sink max current. This is done so that the modules start in a known state and each module is forced to engage in load sharing asap. When LS reaches 80% of required value, ADJ reverts to normal.

    The UCC29002-1 does not have this feature

    Regards

    John