This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

charging solution with 14 serial lithum ion cells

Hi

      The input sources are solar panel, its voltage is 50 to 80v. current (max) 15A..how to charge the battery with 10A curret??   I am looking for its solution..

     Another, solar panel sourc may be used to invertor (dc to ac), and this is prior to charging the battery. how to dynamic  assign current to charge the battery quickly if possible while guarantee the invertor have sufficient input power..

       The battery is 100Ah, so the charging current need  10A, and this battey is used for  ups..

    Best Regards